Technical FAQs

Ask a Question

Power Adaptor of Pretec GSM/GPRS CF Card on Netbotz

Issue:

Power Adaptor of Pretec GSM/GPRS CF Card on Netbotz

Product Line:

NetBotz

Environment:

NetBotz version 2 with Pretec GSM

Cause:

Configuration options.

Resolution:

There is a backup battery with Pretec CF card. However in order for this card to function properly in the NetBotz appliances, the external power must be connected to the card via its power adaptor.
Was this helpful?
What can we do to improve the information ?