Technical FAQs

Ask a Question

BMS AP9921X-AP9922; alarms “Battery Low Chemistry Voltage”

 
 
 
Issue:
BMS AP9921X-AP9922; alarms “Battery Low Chemistry Voltage”

 
Product line:
Battery Management System (BMS) AP9921X & AP9922

 
Environment:
All models, all serial numbers

 
Cause:
The voltage of a battery is below the threshold for the battery type.
 
 
Resolution:
Identify the listed batteries immediately so that system backup time is not reduced. Check for exterior causes of this alarm, such as a loose connection or corrosion on a battery post. If the battery has no external problems, perform a follow-up reading with a battery tester. If a specific battery causes repeated alarms (especially if the voltage continues to decrease), the battery is failing. Replace the battery.
 
 
Was this helpful?
What can we do to improve the information ?