Technical FAQs

Ask a Question

Can I use the ACSC1XX with Hot Aisle Containment System (HACS)?

Issue:
Can I use the ACSC1XX with Hot Aisle Containment System (HACS)?

Product line: A
ACSC1XX

Environment:  
All Serial Numbers

Cause:  
FAQ

Resolution:
No, the HACS ceiling tiles will interfere with the condenser duct tubes. Also in configurations were HACS is required it will make more sense to offer the InRow RC, RD, or RP units.
 
 
.
Was this helpful?
What can we do to improve the information ?