Technical FAQs

Ask a Question

Can I hard wire the ACSC1XX?


Issue:
Can I hard wire the SC? 

Product line:
ACSC1XX

Environment:  
All Serial Numbers

Cause:  
FAQ

Resolution:
 
No, the SC unit must use the power cord provided with the unit
 
Was this helpful?
What can we do to improve the information ?