Technical FAQs

Ask a Question

***ARCHIVE*** Netbotz Basic View for Handhelds Support

***ARCHIVE*** 
To access a NetBotz appliance from a network enabled handheld device, simply point the web browser on the handheld to the hostname or IP address of the Version 2 appliance. The Basic View for handhelds allows handheld WiFi or GPRS enabled devices to access NetBotz Appliances via a web browser.
Supported Devices:
  • Palm OS 5.2.1 Devices:
    • PalmOne devices: Tungsten, Zire
    • Sony devices: Clie`
  • Windows Mobile 2002 or 2003 Devices:
    • HP iPAQ
    • Dell Axim
    • Toshiba e400
  • Blackberry OS 3.7 or higher:
    • Blackberry 6xxx & 7xxx series devices
Was this helpful?
What can we do to improve the information ?