Video: Back-UPS Pro M2 & RS with SineWave; Adjustment of unit battery transfer sensitivity
Issue: APC Back-UPS Pro M2 & RS with SineWave; Adjusting the battery transfer settings.
Product Line:
Back-UPS Pro "M2" and "BR SineWave" models
BR1000MS / BN1100M2 / BN1350M2 / BR1350MS / BN1500M2 / BR1500MS
Cause: UPS is not operating On-line or may be transferring to battery power frequently.
Resolution: The following video details the process for manually adjusting the on-battery transfer thresholds for the Back-UPS Pro M2 & RS with SineWave series. These settings may also be adjusted through PowerChute Personal Edition software on compatible Windows computers.