Technical FAQs

Ask a Question

MAC address Vendor ID of Network Management Cards, and other network devices changing

Issue
APC branded network devices will be using a new vendor indicator in the MAC address


Product Line
  • Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/35CH
Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP7XXXB, AP84XX, AP86XX, AP88XX, AP89XX), Rack Automatic Transfer Switches (AP44XX), Certain Audio/Video Network Management Enabled products, Smart-UPS Online (SRT)
  • SmartConnect UPS
  • Netbotz devices (rack/wall mount, mini sensors)
 
 
Cause
A MAC address is a unique identifer given to a network card when it is manufactured. It can be written in the format MM:MM:MM:UU:UU:UU, where M represents a standard vendor ID (also referred to as an OUI, or Organizationally Unique Identifier)  and U represents a unique identifier for that device.  APC Network devices originally used 00 C0 B7 as the vendor ID, however newer networked devices will be changing that section. 


Resolution
The limit of unique identifiers has been reached in the "00:C0:B7" MAC address range, so a new ID of "28:29:86" is being used. Network protocols that use MAC address (such as static IP's configured via DHCP, or the 802.1x protocol MAC bypass) would need to be updated to include the new APC vendor prefix. Units manufactured in late Q4 2017 will have the new MAC prefix.

The APC Device IP configuration wizard uses the MAC address to identify unconfigured APC network cards. Older revisions of the wizard will not work with cards that use the new vendor ID; IP config wizard v5.0.4 and higher support both vendor ID's.
Was this helpful?
What can we do to improve the information ?