Technical FAQs

Ask a Question

PowerChute Network Shutdown v4.2 not communicating with iReasoning or MG-Soft when authentication protocol is set to SHA 512.

Issue:
PowerChute Network Shutdown v4.2 not communicating with iReasoning or MG-Soft when authentication protocol is set to SHA 512

Product Line:
PowerChute Network Shutdown version 4.2

Environment:
PowerChute Network Shutdown version 4.2 configured with NMS tool iReasoning or MG-Soft
 
Cause:
SNMPv3  profile created with SHA 512

Solution:
Create profile with SHA 256 
Was this helpful?
What can we do to improve the information ?