How to Reset the Password for Data Center Operation Server?
Issue:
How to Reset the Password for Data Center Operation Server?
Product Line:
Data Center Operation (DCO)
Environment:
Data Center Operation 8.x (DCO)
Cause:
If the password for logging into the Data Center Operation Server for either command-line console or the Webmin web interface is lost or forgotten.
Resolution:
To reset the password of Data Center Operation Server for either Webmin or the command line console please see the following DCIM Support article: