Technical FAQs

Ask a Question

What size wrench is needed to remove the NetShelter pallet bracket?

Customer may ask what size the pallet bracket bolts are.

Product Line:
NetShelter SX, NetShelter SV, NetShelter VX

All versions and serial ranges.

Customer wants to make sure they have the proper tools on hand.

NetShelter SX, SV and VX pallet brackets require a 13 mm wrench.
The NetShelter SV also requires a T30 Torx wrench (included). If the bolts are too tight for the included T30 Torx tool please use a T30 Torx socket and socket wrench.
Was this helpful?
What can we do to improve the information ?