Technical FAQs
Technical FAQs
Issue:
How to clean Heatcraft-Larkin Refrigeration condensers
Product line:
Heatcraft Condensers, LNE, FCB, KH1,SCS, LNH,
Environment:
All Product models, all serial numbers
Cause:
(Backspace and type high level possible cause of failure symptom or alarms)
Resolution:
Maintenance
Air cooled condensing units require a minimum of maintenance. The unit coil will require a periodic cleaning and this can be accomplished by a brush, vacuum cleaner, pressurized airstream or a commercially available coil cleaning foam. All of the condenser fan motors have sealed ball bearings. The only acceptable service to these bearings is replacement.
Cleaning Instructions
Heatcraft recommends that the finned surface of this unit be cleaned approximately every six (6) months; more frequent cleaning may be required if extreme conditions cause clogging or fouling of air passages through the finned surface. Calgon Corporation's CalClean 41352 (or equal) should be acceptable for cleaning this unit. CalClean should be applied liberally to entering air and leaving air surfaces of the finned area in accordance with the label directions.
CAUTION: Under no circumstances should this unit be cleaned with an acid-based cleaner.
Reference Heatcraft-Larkin Refrigeration Products Remote Air Cooled Condensers Manual. Bulletin H-IM-73A June 2000 Part Number 90800801