Are there baying brackets available for the NetShelter VX Seismic cabinets?
Issue:
Customers may want to bay together NetShelter VX Seismic cabinets.
Product Line:
NetShelter VX Seismic
Environment:
All versions and date ranges.
Cause:
Customers may want to use baying brackets to enhance the seismic feature, or to help align rows of cabinets.
Resolution:
There are no baying brackets for the NetShelter VX Seismic cabinets.
The NetShelter VX Seismic cabinets are designed to be mounted to the floor in NEBS GR-63-CORE seismic installations, and baying brackets are not necessary. Baying brackets do not enhance the seismic feature of the cabinet.