Technical FAQs

Ask a Question

Messaging is not available on PowerChute Business Edition running on Microsoft Vista and above.

PowerChute Business Edition messaging option is not available on  Microsoft Vista and above.

PowerChute Business Edition

Microsoft Vista above

This is a Microsoft limitation. Microsoft has omitted the messenger service that it has used since Windows NT. This is the background process that PowerChute has been using to message the local server as well as remote servers.


 PowerChute Business Edition is capable of running command files so if you have an alternative messaging system on your computers that can be called from a command/batch file, you may be able to use this as a solution. For help writing command files for use with PowerChute Business Edition please review Kbase FA168226
Was this helpful?
What can we do to improve the information ?