Technical FAQs

Ask a Question

What is the AR8395 Busbar Amp rating?

Issue:
What is the Amp rating for the AR8395 busbar?

Product Line:
NetShelter Accessories
 
Environment: 
AR8395
 
Cause:
Equipment in the NetShelter must be grounded.
 
Resolution:
See attached document, or explanation below.
 
AR8395 Busbar Amp Rating

As of this writing (April 2012)  the AR8395 busbar has not been rated for power grounding. It is designed for low voltage applications. Its intended use is to ground equipment chassis of switches, routers, AV and other low voltage IT equipment to reduce noise from the system. Because of this intended use the AR8395 Busbar has not been rated for amperage. Should this product be rated in the future this document will be updated.

Was this helpful?
What can we do to improve the information ?