Technical FAQs

Ask a Question

Configuring SeaLevel 450 Relay I/O Device within Netbotz

Issue:

Configuring SeaLevel 450 Relay I/O Device within Netbotz

Product Line:

NetBotz
Sealevel

Environment:

NetBotz version 2 and 3
Sealevel 450

Cause:

3rd party device configuration.

Resolution:

Once the I/O Device is connected to the Appliance, configuration for the Seal/O device can be done by the following:

1. Launch the Advanced View on the Appliance.
2. Double click the 'Serial Devices' Applet
3. In the drop-down menu, select the Sea-Level Product >> SeaLevel SeaI/O 450.
4. Then select 'OK'


Was this helpful?
What can we do to improve the information ?