Technical FAQs

Ask a Question

Dew-Point Calculations on the NetBotz Appliances

Issue:

Dew-Point Calculations on the NetBotz Appliances

Product Line:

NetBotz

Environment:

NetBotz version 1 and 2

Cause:

Definition: Dew Point is the temperature at which condensations forms

Resolution:


When air comes in contact with a surface that is at or below its Dew Point temperature, condensation will form on that surface.

The following URL explains how the dewpoint is calculated:

http://www.lamtec.com/tb_dew_point_calculator.html

Was this helpful?
What can we do to improve the information ?