Technical FAQs

Ask a Question

What is the difference between SYBT5 and SYBT5FR?


The main difference is that the SYBT5FR sku has batteries with flame retardant rated plastic. These are required in Japan. Unless the flame retardant specification is required the standard SYBT5 is recommended for use with Symmetra LX.

Was this helpful?
What can we do to improve the information ?