Technical FAQs
How do I perform a mass firmware upgrade on APC network enabled products?
Issue
How can I upgrade firmware on multiple APC Network Management Cards at one time or in an automated fashion?
Product Line
- Network Management Card 1 (NMC1) - AP9617, AP9618, AP9619
- Network Management Card 2 (NMC2) - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/AP9635CH
Environment
- All serial numbers
- All firmware versions, unless otherwise noted
Cause
A user may wish to automate the process of upgrading firmware on Network Management Cards or devices with an embedded card to save time, especially with large quantities of devices.
Resolution
Users can upgrade the firmware on individual Network Management Cards via a couple of different methods, specifically
- FTP
- SCP
- XMODEM
- Infrastruxure Manager (discontinued product)
- StruxureWare DCE/InfrastruXure Central
- Upgrade Executable/Wizard (the executable is included with the firmware when downloaded)
- USB (if available)
In some cases, a user may have multiple devices that need to be upgraded. The user can upgrade each device individually. However, this may prove to be time consuming.
Therefore, the user has two options to perform a mass upgrade of firmware.
- The first, Infrastruxure Manager, is a discontinued item that monitors APC network enabled devices. A feature of the Infrastruxure Manager is the ability to perform mass firmware upgrades. Please reference the user’s manual or help menu for the Infrastruxure Manager to perform the mass firmware upgrade. Infrastruxure Central/StruxureWare Central/StruxureWare DCE is Infrastruxture Manager's replacement and offers this feature as well.
- The second, the Upgrade Executable which is included with all currently downloaded firmware for both Network Management Card 1 and 2 devices as well as those that embed one of these model cards. You can obtain the latest firmware from the following web site:
http://www.apcc.com/tools/download/
Download the firmware to your local computer. An example of the firmware that you download will appear as:
apc_hw02_aos374_rpdu374.exe
Once downloaded, you can run this file and it will automatically launch one of two executables, depending on which firmware you have downloaded.

Network Management Card 1 devices
Once you execute the firmware file .exe, you'll be prompted to extract the files to a chosen location or directory.
Once extracted, the executable will attempt to run the upgrade. Simply close the command prompt windows that open. Locate the directory that the extracted files were saved to. In this directory, you should see a file named “iplist.txt”. Open this file in a text editor. The contents on the iplist.txt should appear similar to:
;SystemUserName=username (the username of the device you with to upgrade)
;SystemPassword=password (the password of the device you with to upgrade)
Note: Any lines in the iplist.txt file starting with a semicolon will be ignored.
SystemUserName=apc
SystemPassword=apc
SystemIP=192.168.1.2
SystemUserName=apc
SystemPassword=apc
Once you have entered the login parameters for each device, make sure to save and exit the file.
Next, locate the “upgrd_util.exe” file, also located in the same directory that you extracted the firmware files to. Double-click on the “upgrd_util.exe” file and the mass upgrade will begin.
Note: *In NMC1 Upgrade Utility v1.2 or higher, a username or password longer than 11 characters will be truncated. Thus, you will need to change the password to 11 characters or less to use upgrd_util.exe. This could be modified using a mass configuration first, outlined in knowledge base FA156117. Reference the picture below on how to check your NMC Upgrade tool version.
A menu should appear with the following options:
1. Use parameters in configuration file.
2. Enter parameters for single upgrade.
3. Exit firmware upgrade tool.
Choose option 1.
The firmware upgrade will now begin. The executable will attempt to upgrade all devices listed in your IP list. If any errors are found, the upgrade will continue on to the next device.
Network Management Card 2 devices
On the Network Management Card 2 executable utility that automatically launches after files are extracted (FW_Upgrade_R2.exe), press the "Device List" button which will open iplist.txt in your default text editor.
Alternatively, locate the directory that the extracted files were saved to and in this directory, open the file named iplist.txt manually in a text editor. The contents on the iplist.txt should appear similar to:
; Copy, paste, and modify one entry for each device in your network.
; Lines with leading semicolons (;) are considered comments.
; Note: Order and spacing are important and need to be the same as the example.
The below portion is in v2.20 Firmware Upgrade Utility or higher only (this actual text instruction, IPv6 support, and downgrade support). Check the previous screenshot to compare your program title bar and see if it says v2.20 or higher. If it only says Firmware Upgrade Utility, it is older.
; SystemIP is the IPv4 or IPv6 address of the device
; SystemUserName is the name of an enabled Administrator or higher account on the NMC
; SystemPassword is the password of an enabled Administrator or higher account on the NMC
; AllowDowngrade can be 0 for disabled (do not allow) or 1 for enabled (allow) for firmware downgrades
; SystemIP=192.168.0.1
; SystemUserName=apc
; SystemPassword=apc
; AllowDowngrade=0
; SystemIP=192.168.0.2
; SystemUserName=apc
; SystemPassword=apc
; AllowDowngrade=1
Once you have entered the configuration for each device, make sure to save and exit the file. (APC recommends no more than 10 devices at one time). On the Network Management Card 2 executable, select the checkbox that says Upgrade from Device List and then press Upgrade Now to begin the upgrade. See below.
Once the upgrade is complete, you will be required to close the executable/command prompt window.
If you have any questions on this process or experience trouble, please contact APC technical support. Before calling, please have the following information available:
-
Firmware that you downloaded.
-
Which method are you using?
-
Device model and serial number that you are attempting to upgrade
-
What type of error do you receive when attempting to upgrade?
-
How many devices are you attempting to upgrade?