Technical FAQs

Ask a Question

Filter results

Clear
How to configure NetBotz version 2 external sensors?
Issue: Netbotz External Sensor Installation Tips Product Line: Netbotz Environment: NetBotz 2.x Cause: Configuration tips. Resolution: Adding sensors...
Disabling Audio Recording on the Model 500
Issue: Disabling Audio Recording on the Model 500 Product Line: Netbotz Environment: NetBotz NBWL0500 Cause: The NetBotz 500 has the ability to record...
NetBotz 500 Amperage Information
Issue: NetBotz 500 Amperage Information Product Line: Netbotz Environment: NetBotz 500 Cause: Current draw Resolution: NetBotz 500 Amperage Information...
Is there a limit to the number of e-mail addresses that can be configured to receive alerts from a NetBotz device?
Issue: Is there a limit to the number of e-mail addresses that can be configured to receive alerts from a NetBotz device? Product Line: NetBotz Environment:...
Physical Sizes of Camera Pod 120 and Sensor Pod 120
Issue: Physical Sizes of Camera Pod 120 and Sensor Pod 120 Product Line: NetBotz Environment: NetBotz Version 2 camera pod NBPD0121 Cause: Physical...
Configuring the Return or Reply Email Address on a Netbotz Appliance
Issue: Configuring the Return or Reply Email Address on a version 1 Netbotz Appliance Product Line: NetBotz Environment: NetBotz version 1 and 2 Cause:...
NetBotz location information not retained on Pelco camera after reboot.
Issue: NetBotz location information not retained on Pelco camera after reboot. Product Line: NetBotz Pelco Cameras Environment: Botzware version 4.2...
Temperature and Humidity Sensor Specifications for Version 1 Appliances
Issue: Temperature and Humidity Sensor Specifications for Version 1 Appliances Product Line: NetBotz Environment: NetBotz version 1 appliances Cause:...
Is there RoHS or REACH documentation available for NetShelter cabinets and accessories?
Issue: Customers need a copy of our RoHS or REACH document. Product Line: NetShelter SX cabinets and Accessories. Environment: All versions and serial...
Why are the Dell ReadyRails II loose?
Issue: The customer is having difficulty installing Dell ReadyRails II into a NetShelter cabinet.  Product Line: NetShelter SX, VX, SV, CX Environment: ...
Results 1 - 10 of 100