Technical FAQs

Ask a Question

Can a short depth SMX Smart-UPS and SMX battery be installed into a NetShelter AR100 or AR100HD?
Issue:  The cord will connect but the rear door won't close. If it's forced closed the power cord can separate from the molded cable end exposing...
Video: How to install PowerChute Business Edition versions 9.0 to 9.2.1
Issue: How to install PowerChute Business Edition UPS monitoring software  Product: PowerChute Business Edition versions 9.0 to 9.2.1 Environment:...
How to set self test day and time on Symmetra UPS products
Issue: How to set self test day and time on Symmetra UPS products   Product line: Symmetra PX, Symmetra PX2, Symmetra LX, Symmetra RM   Environment:...
Do the 800 mm wide NetShelter SV cabinets have 1U rackmount spaces in the vertical mounting rails?
Issue:  This space would be perfect to mount small IT devices into.  Product Line:  NetShelter SV  Environment:  800 mm width only, all serial numbers. ...
Is the PDU removable that's included inside the NetShelter CX AR4000MV?
Issue:  A customer wants to replace the PDU in a NetShelter CX Mini.  Product Line:  NetShelter CX Environment:  AR4000MV, all serial numbers.  Cause: ...
Downloading the MIB file for version 3 Netbotz.
Issue: Downloading the MIB file for version 3 Netbotz. Product Line: NetBotz Environment: NetBotz version 3 MIB Cause: Obtaining the NetBotz version...
StruxureWare DCE Does Not Boot After Importing SSL Certificate Chain.
 Issue Importing an SSL certificate chain into StruxureWare DCE prevents the web server from starting, making the StruxureWare DCE unable to boot....
NetBotz TFTP upgrade procedure.
Issue: NetBotz TFTP upgrade procedure. Product Line: NetBotz version 3 Environment: NetBotz model: 355, 455, 450, 550,  570. Cause: Optional NetBotz...
Is there an offset baying bracket or some way to bay cabinets of different depths?
Issue:  A customer is looking for an offset baying bracket for NetShelter SX cabinets.  Product Line:  NetShelter SX Environment:  All models, all...
What size bolts are needed to floor mount the NetShelter 4-post rack?
Issue:  A customer needs to know what size bolt will fit through the floor mounting holes in the rack.  Product Line:  NetShelter SX Environment: ...
Results 1 - 10 of 100