{}

Our Brands

Search FAQs

Video: Data Center Expert | How do I configure auto-login when launching to APC devices?

Issue:
How do I configure auto-login when launching to APC devices within the StruxureWare Data Center Expert desktop client?

Product Line
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)

Environment
StruxureWare Data Center Expert (all versions)
StruxureWare Central (all versions)
InfraStruXure Central (all versions)

Cause:
Double clicking on an APC device (NMC) in StruxureWare DCE launches a browser window to that device automatically logging in if configured correctly.

Resolution:



1) Open the DCE desktop client and navigate to: Monitoring perspective > Device View pane.
2) Right-click on an APC device and select Device Launch settings. Use Ctrl+click or Shift+click to select multiple devices at once.
3) Ensure that the correct protocol, port, username, and password are defined for accessing the devices web interface.  Select OK.
4) Double-click on the device, or right-click and select Launch to Device, and the web interface of the device should load and automatically log in.

APC USA

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.