Technical FAQs

Ask a Question

NetBotz Central 2.x - Graph Color Legend are Incorrect


NetBotz Central - Graph Color Legend are Incorrect

Product Line:

NetBotz Central


NetBotz Central 2.x


When color boxes in the table of a graph view are all white boxes, users cannot distinguish which line corresponds to which sensor


This is typically tied to the client settings, and can usually be corrected by going to "Edit->Preferences", then in "Appearance" switch to a non-Windows "Look and Feel" (In NBC v2.1.x, it is called "Toolbar"), and close and re-open the NetBotz Central console.
Was this helpful?
What can we do to improve the information ?