Technical FAQs

Ask a Question

Altering the Image Orientation on Netbotz

Issue:

Altering the Image Orientation on Netbotz

Product Line:

NetBotz

Environment:

NetBotz all versions.

Cause:

Alternative configuration.

Resolution:

The image orientation can be altered on all appliances. Simply check the box under Camera Configuration that says ""Rotate Camera Image"". This will rotate the image 180 degrees to allow a camera that is mounted upside down to be displayed properly in the Advanced View or Basic View. 
Was this helpful?
What can we do to improve the information ?