Technical FAQs

Ask a Question

Display of hostname on ISX Central/Netbotz Central map view


Display of hostname on InfraStruxure Central/Netbotz Central map view

Product Line:

InfraStruxure Central/Netbotz Central


Any version


Hostname information


Hostname can be set as the tag but the hostname and IP address need to be resolvable in the local DNS server. Once that is done, go to the Central's tools/preferences menu and click on general and change display device to read hostname

Was this helpful?
What can we do to improve the information ?