Technical FAQs

Ask a Question

Launching Advanced View Targeted at Specific Appliance

Issue:

Launching Advanced View Targeted at Specific Appliance

Product Line:

NetBotz

Environment:

NetBotz Advanced View 2.3 and higher, 3.x, and 4.x

Cause:

Alternative launching options for NetBotz Advanced View Software.

Resolution:

You can launch the NetBotz Advanced View version 2.x targeted at a specific appliance by using the -s option with the Advanced View executable.

Examples:
"NetBotz Advanced View 2.3.exe" -s http://192.168.17.100
"NetBotz Advanced View 2.3.exe" -s https://bothostname.com

The full path may also be necessary
C:\Program Files (x86)\Advanced View 4.2.0\Advanced View.exe -s http://192.168.10.101

Was this helpful?
What can we do to improve the information ?