Technical FAQs

Ask a Question

AIS3000 External Battery Frame

"The AIS3000 can be attached to External Battery Frames in order to increase the runtime.

The maximum number of External Battery Frames is limited to 4 due to the recharge time.

There are 2 different External Battery Frame models depending on whether the frame has Circuit Breaker integrated or not.

2-External Battery Frames for AIS3000

XR Frames with Circuit Breaker:



XR Frames without Circuit Breaker:



Was this helpful?
What can we do to improve the information ?