Technical FAQs

Ask a Question

Are NetShelter SV cabinets compliant for seismic installation?

Issue: 
The customer would like to know if the NetShelter SV cabinets are rated for seismic installations in UBC High Seismic Area or OSHPD. 

Product Line: 
NetShelter SV

Environment: 
All versions and serial ranges 

Cause: 
A customer is looking for a seismic rated cabinet. 

Resolution:   
The NetShelter SV cabinets are not rated for seismic installation. There are no brackets or accessories that can make them compatible for a seismic installation. 
Was this helpful?
What can we do to improve the information ?