Technical FAQs

Ask a Question

What is the rack depth within the NetShelter CX or CX Mini?

Issue: 
Customers need to know how deep the rails of the NetShelter CX are.
 
Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
Customers want to make sure that their equipment will mount into the cabinet.  
 
Resolution :
see below
  
NetShelter CX Mini has an available equipment depth of 700mm/27.5” in standard format. With the optional accessory 12U Rack Kit for Mini (AR4000MV12U) installed there is an equipment depth of 600mm/23.6”.
All NetShelter CX2 models (AR40xxA, AR40xxIA) have adjustable front and rear posts. Rack depth is 800mm / 31.5” adjustable down to 118mm / 4.75”.  
All NetShelter CX models (AR40xx, AR40xxI) have adjustable front rack posts. Rack depth is 800mm / 31.5” adjustable down to 700mm / 27.5”.
Was this helpful?
What can we do to improve the information ?