Technical FAQs

Ask a Question

How do I update the firmware of my SMT, SMX, SMC, or SRT series Smart-UPS?

Issue: 

Next generation Smart-UPS products feature user upgradeable UPS Firmware.
This allows for ongoing improvements and feature enhancements of Smart-UPS products after deployment.
 
 

Product line:

Smart-UPS SMT, SMX, SMC, and SRT Families


 

Environment:

Since we will continually release new products that are supported by the tool, we identify devices that are NOT supported.

Devices that are *NOT* supported by the Firmware Upgrade Wizard:

  • UPS-Link Devices: Models beginning with: SU, SUA, SUM, SURT, SURTA, SRC (IE: SUA3000XL, SU2200NET)
  • Microlink Devices: Models beginning with SURTD (IE: SURTD3000XLT)
  • SMX Devices: SMX750, SMX1000, SMX1500 with firmware UPS 02.x or lower. (These units are 120 V devices built prior to date code 1037)
 
The system requirements for the Firmware Upgrade Wizard are as follows:
Operating systems: Microsoft Windows XP®, Windows Vista® , Windows 7®, Windows 8®, 8.1®, and Windows 10®
 
 

Resolution:

There are two methods to update the firmware of the UPS:
  • Locally via a Serial or USB connection using the Firmware Upgrade Wizard application. This is the most reliable method and should be used whenever possible. 
  • Remotely via the Network Management Card
‚Äč
Both methods require that your turn off the output power of the UPS. 
If you are updating via the Network Management Card, you must ensure that your network access is not dependent on the UPS for power.



Smart-UPS models beginning with "SMT", "SMX", or "SMC":
CLICK HERE to upgrade using a Serial or USB connection and the Firmware Upgrade Wizard. (RECOMMENDED)
CLICK HERE to upgrade using the Network Management Card

Smart-UPS models  beginning with "SRT":
CLICK HERE to upgrade using a Serial or USB connection and the Firmware Upgrade Wizard. (RECOMMENDED)
CLICK HERE to upgrade using the Network Management Card

 
Was this helpful?
What can we do to improve the information ?