Technical FAQs

Ask a Question

How can I view/export PowerChute Business Edition and PowerChute Network Shutdown log files?

Issue:
How can I view/export PowerChute Business Edition and PowerChute Network Shutdown log files?

Product:
PowerChute Business Edition
PowerChute Network Shutdown

Environment:
All support OS

Solution:

For PowerChute Business Edition(PCBE):
The data log exists in the file <agent path>\DataLog on Windows system or <agent path>/DataLog on Unix/Linux system.

For PowerChute Network Shutdown(PCNS):
The event log exists in the file <install path>\groupn\EventLog.txt on Windows system or <install path>/group1/EventLog.txt on Unix/Linux system.

You can view the DataLog of PowerChute Business Edition and EventLog.txt of PowerChute Network Shutdown in the user interface. To open those logs with other applications, please navigate to the directory that the files reside and then open with other applications like wordpad, notepad, Excel or VI etc.
NOTE: You can only view PowerChute Business Edition event log with PowerChute Business Edition user interface. You can copy and past the event log into another application if required.
 
Was this helpful?
What can we do to improve the information ?