How to calibrate sensors on version 2 NetBotz appliances?
Issue:
Calibrating Sensors on NetBotz version 2 Appliances
Product Line:
NetBotz
Environment:
Version 2 NetBotz sensors
Cause:
Questionable readings from sensors may suggest that devices require calibration.
Resolution:
As a general rule, sensors (temperature, humidity, and airflow) on version 2 NetBotz Appliances DO NOT need to be calibrated. All of the electronics sensors used by NetBotz appliances are fully calibrated by the supplier.
Please remember the temperature readings have a 1.8 to 3.6 degree F (1 degree C to 2 degrees C) accuracy range depending on the model. Humidity sensor accuracy ranges from 5% to 10% depending on the model.
If you feel your appliance is not accurately reporting temperature and humidity readings correctly, please contact NetBotz Support.