UGANDA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
UGANDA - Choose Country or Region
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
Manual Upgrade process for Version 1 Appliances
Issue:
Manual Upgrade process for NetBotz Version 1 Appliances
Product Line:
NetBotz
Environment:
NetBotz version 1
Cause:
Firmware upgrade procedure..
Resolution:
Please Note that all version NetBotz appliances are end of life and end of support.
Manual Upgrade process for Version 1 Appliances
This article outlines the manual upgrade procedure for all Version 1 Appliances (300, 303, 310, 400).
--Download & unzip the latest version of the firmware for the Version 1 Appliances.
--Find the appropriate rom.bin file for the type of appliance you are upgrading.
*************************NOTE*********************************************************
Note that:
--The directory "releases_300" is for 300/303 models
--While the directory "releases" is for the 310/400 models.
****************************************************************************************
--Open a command / DOS prompt in the directory where the appropriate rom.bin file is located.
--Now follow the commands below once you've located the appropriate file:
1. ftp <botz ipaddress> (where <botz ipaddress> is the ip address of the botz unit)
(Login with supervisor acct)
2. quote eraseapp
3. quote reboot
4. quit
Proceed to perform a second ftp session into the Botz device.
1. FTP <botz ipaddress>
(no username/password required)
2. bin (this puts the bot in "Binary" mode
3. put rom.bin (transfers the file/OS to the bot)
4. quote reboot (tells the bot to apply the software after rebooting)
5. quit
--Once the appliance restarts for the final time, it will then be available for usage.
--Browse to the bot and install the latest version of the Advanced View Software.
--This can be downloaded at the following link:
http://www.netbotz.com/support/index.html#installers
Please be aware that the version 1 NetBotz are End Of Life an no new releases will be developed.
See Knowledge Base document # FA158097