Technical FAQs

Ask a Question

User Access Levels for Version 2 Appliances

Issue:

User Access Levels for Version 2 Appliances

Product Line:

NetBotz

Environment:

NetBotz version 2 and 3

Cause:

Each appliance can have multiple user IDs for granting access to different admins and users. There are 6 levels of user access that can be assigned to user IDs created on the appliance:

Resolution:


* Administrator: Gives user access to all information and configuration tasks available on the appliance.
* Application with alert update: Gives user access to only the Navigation, Sensor Data and selected portions of the Information/Action panes. User accounts configured with the Application Privilege Set can view the Camera, Graphs, Alerts, and About panes. The user can also resolve alert conditions for thresholds that have been configured with the Return-To-Normal Requires User Input setting in their Advanced Settings.
* Application: Gives user access to only the Navigation, Sensor Data and selected portions of the Information/Action panes. User accounts configured with the Application Privilege Set can view the Camera, Graphs, Alerts, and About panes.
* Sensor: Gives user access to only the Navigation, Sensor Data and selected portions of the Information/Action panes. User accounts configured with the Sensor Privilege Set can view the Camera, Graphs, and About panes.
* Sensor no camera: Gives user access to only the Navigation, Sensor Data and selected portions of the Information/Action panes. User accounts configured with the Sensor (No Camera) Privilege Set can view the Graphs and About panes.
* None: Does not permit access to any appliance features (disables access). 
Was this helpful?
What can we do to improve the information ?