Technical FAQs

Ask a Question

Video: Symmetra Power Array Module Replacement Procedure


Issue

I need to install or replace a module in my Symmetra Power Array UPS system.  How do I do this?


Product Line

Symmetra Power Array


Environment

All serial ranges


Cause

Symmetra UPS are designed with modularity so that modules can be added or replaced as needed.  This document contains a video to aid the user in performing the installation of a new module or replacement of an existing module.


Resolution

The following video details the process of replacing the Intelligence, Battery, and Power Modules in the Symmetra Power Array UPS.
 


 
Was this helpful?
What can we do to improve the information ?