Technical FAQs

Ask a Question

What are the standard output receptacles for the Matrix UPS line?

The Matrix comes standard with (6) 5-15 receptacles, (2) L6-30 receptacles and (1) L14-30 receptacles.
Was this helpful?
What can we do to improve the information ?