Technical FAQs

Ask a Question

What third party products are supported by the APC Netbotz SNMP Crawler?

"The APC Netbotz product range has SNMP crawler support for APC products, MGE products, as well as third party manufacturers. Listed below are major manufacturers supported by the SNMP crawler with a list of common supported products broken down by manufacturer below.

APC
Alcatel
Avaya
Best Power
Cisco Systems
Compaq
DMTF
Dell
Extreme Networks
Foundry Networks
IBM
Juniper Networks
Liebert
MGE
MIB2-UPS
Mitsubishi
NetBotz
Powerware
Sun Microsystems

Liebert

Info from: http://www.liebert.com/dynamic/displayproduct.asp?id=921&cycles=60hz
And http://www.liebert.com/products/english/products/site/com_nic/comp.asp

UPS
AP 200 UPS
Series 300/301 UPS
AP 4300
Series 600 System Control Cabinet
Series 600 Single Module System UPS
UPStation D/Select UPS
UPStation G/GX/GRT/Gold
UPStation GXT
PowerSure Interactive
UPStation S UPS
UPStation S3 UPS
NPower
Hiross 7200 (Italy)
Hiross HiPulse (Italy)

Environmental Products
Deluxe System 3
Challenger
MiniMate 2
Level 00/05/10/15
Himod

3-Phase Power
DataWave
Static Switch
Static Switch 2


MGE

Pulsar Evolution
Pulsar EX
Pulsar EX RT
Comet EXtreme
Comet EXt RT
Comet 3000
Comet S31
Galaxy
Galaxy 1000 PW
Galaxy 3000
Galaxy 4000
Galaxy PW Harmony
Galaxy PW
EPS 6000
EPS 8000


Eaton Powerware

Info from: http://www.powerware.com/ups/connectivity/connectups_snmp.asp
And http://www.powerware.com/ups/connectivity/ConnectUPS_SL_SNMP.asp


Powerware 9155
Powerware 9315
Powerware 5119
Powerware 9 Prestige
Powerware 9150


Mitsubishi UPS
Info from: http://www.meau.com/eprise/main/sites/public/PRODUCTS/Uninterruptible_Power_Supplies/NetCom/default

2033A Series
2033C Series
2033D
7011A Series (1kVA to 3kVA, 6kVA to 12kVA)
9700 Series
9800D Series

Best
Info from: http://www.powerware.com/UPS/BestPower/Products.asp

Fortress
Patriot Pro
FERRUP
Best Power 610"
Was this helpful?
What can we do to improve the information ?