Technical FAQs

Ask a Question

Video: How to change a Cooling Set point on a push button Uniflair display

Issue:
How to change a cooling set point on a Uniflair Unit.
 
Product line:
All Uniflair Units with Push-Button Display, All Chilled Water Uniflairs.
 
Environment:
All Serial Number with Push-Button Units.
 
Cause:
Repair, Install, Maintenance.
 
Resolution
 
How to change a Cooling Set point on a push button Uniflair display.
 
Press <> PRG.
 
Settings Menu <> ENTER.
 
Code <> 00000 ENTER.
 
Operative settings <> ENTER.
 
Press ENTER again to the cooling set point.
 
Use the Arrows to set the correct temperature.
 
Press ENTER twice and then ESC back out to the main menu.
 
 
 
Was this helpful?
What can we do to improve the information ?