TANZANIA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
TANZANIA - Choose Country or Region
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
How do I configure the date/time on a v3 NetBotz Appliance?
Issue:
Process for configuring date/time settings on a v3 NetBotz Appliance.
Product Line:
NetBotz version 3
Environment:
NetBotz Model: 355, 455, 450, 550, or 570.
Resolution:
1) Log into the
Advanced View
application using an Administrator account.
2) Select the
Configuration Tab
and then under Appliance Settings select
Clock
.
Proceed with setting up Network Time Protocol (NTP) or manually defining the date/time.
Configuring Date/Time using NTP
3)
Check
the Box for
Enable NTP
.
4) Define the
Primary NTP Server
hostname or IP Address you would like to use.
NOTE:
You can add up to three NTP servers.
5) Select
Set time now using NTP
to force sync the date and time with the NTP server(s).
6) Select
OK
.
Configuring Date/Time Manually
NOTE:
It is recommended to configure the Date/Time using NTP whenever possible.
3) Ensure the box is
unchecked
for
Enable NTP
is not checked.
4) Manually define the
Date/Time
.
5) Click
OK
.