Technical FAQs

Ask a Question

Video: How to change the Coil Fluid Temperature Thresholds on a Network Air FM Unit

Issue:
How to change the Coil Fluid Temperature Thresholds on a Network Air FM Unit.
 
Product line:
FM 35-50, IR40, ACFM400, ACFM200.
 
Environment:
All Serial Numbers.
 
Cause:
Install, Configuration.
 
Resolution:



To change or set the coil fluid temperature threshold.

Press the ESC Key until you get to the main menu.

Press ENTER on Setup.

Press ENTER on System 1.

Press ENTER on Alarms.

Scroll down to Coil Fluid Thrshlds and press ENTER.

Using the UP or DOWN arrows you can select the High or Low threshold.

Press ENTER on either then change the value with the UP or DOWN arrow.

Finish by pressing the ENTER key and then press ESC until you get to the status menu.
 
Was this helpful?
What can we do to improve the information ?