Technical FAQs

Ask a Question

Can a 63.75" tall PDU be installed into a 38U NetShelter CX cabinet?

Issue:
The 63.75" tall PDU does not fit onto the accessory rail. Will it fit anywhere else inside the cabinet? 

Product Line: 
NetShelter CX 

Environment: 
AR4038A, AR4038IA

Cause:
A customer wants to install one of the 63.75" tall PDUs into a 38U NetShelter CX cabinet. 

Resolution:
Yes, the 63.75" tall PDUs can attach to the rear mounting rail. Please see the attached file for mounting instructions. 
Was this helpful?
What can we do to improve the information ?