Technical FAQs

Ask a Question

What is the power consumption of the fans in the NetShelter CX?

Issue:
A customer needs to know how much power is consumed by the NetShelter CX fans.

Product Line:
NetShelter CX
 
Environment:

All versions and serial ranges.
 
Cause:
Customers may need to calculate total power consumption
 
Resolution:
 
NetShelter CX Mini = 30W
NetShelter CX/CX2 18U = 34W
NetShelter CX/CX2 24U = 68W
NetShelter CX/CX2 38U = 101W
 
Was this helpful?
What can we do to improve the information ?