Technical FAQs

Ask a Question

Maximum Size of SMS Message / Alert

Issue:

Maximum Size of SMS Message / Alert

Product Line:

NetBotz

Environment:

NetBotz SMS messaging via GSM modem

Cause:

Message size limitation..

Resolution:

The maximum size of an SMS text message sent via GSM is 160 single byte characters. Different carriers could potentially put lower limits.

Was this helpful?
What can we do to improve the information ?