Standard Lens Specifications for the WallBotz 320 & 420
Issue:
Standard Lens Specifications for the WallBotz 320 & 420
Product Line:
NetBotz
Environment:
NetBotz 320 and 420 Camera
Cause:
Standard Lens specifications.
Resolution:
* Manufacturer: Senview
* Model: TN0416F
* Size: ¼” format
* Focal Length: 4mm
o The focal length distance between the lens and the imager.
* F-Stop: 1.6
o The f-stop affects depth of field, or how much is in focus in front of and behind the subject.
* Field of View (horizontal x vertical in degrees): 48 x 37