Environment:
Supported operating systems for the relevant PowerChute Network Shutdown versions in Product Line above.
Cause:
An SSL handshake error occurs when Java 7 and 8 is installed on the system and PowerChute attempts to communicate with an AP9617, AP9618, AP9619.
Solution:
To correct the issue change the communication protocol between the NMC and PowerChute to HTTP. There is no HTTPS solution with PowerChute Network Shutdown versions 3.1 and 4.x