Technical FAQs

Ask a Question

How to place a ACRD600/ACRD600P unit into On/Standby Mode

Issue:
Standby
 
Product line:
ACRD600, ACRD600P, ACRD601, ACRD601P
 
Environment:
All Serial Numbers
 
Cause:
Install, Repair
 
Resolution
 
This video shows how to place an ACRD6XX/ACRD6XXX unit into On or Standby Mode
 
Press the Home Tab
Press the Unit On/Standby Tab
Press the Right Arrow to select Standby or On
Confirm, and enter the PIN if requested (default PIN is 1234)
Press Ok
Press Home Tab
 
Was this helpful?
What can we do to improve the information ?