Technical FAQs

Ask a Question

What are the system requirements for the StruxureOn Gateway?

System requirements for the StruxureOn Gateway?

Product Line

StruxureOn Gateway


On this page:


  • A server with Microsoft® Windows® 64-bit operating system
  • At least 8 core and 8 GB of RAM
  • 20 GB hard disk space

StruxureOn Gateway 1.0.0 was tested on Microsoft Windows Server 2008 R2 SP1 and Server 2012 SP1. The application takes 225 MB of disk space and the server retains a maximum of 8 days of data, about 700 MB per day.



  • Port 443 TCP outbound
  • To connect using static IPs, add and

Supported browsers

  • Microsoft Internet Explorer®10, 11
  • Mozilla®Firefox®39.0
  • Google Chrome™43.0
  • Safari

Set the screen resolution to at least 1024 x 768.


  • iPhone 4S and newer

  • iOS 8.0 and newer

  • Android 4.4 and newer


Connected devices

  • Intelligent Network Management Card
  • Modbus TCP or SNMP V1 and V3 enabled
  • Connected to a TCP/IP network that the Gateway has access to


Security certificate

When you launch the StruxureOn Gateway, the browser might display a message that the connection is not secure. Since the application is installed on the local machine, the security certificate used by localhost is a self signed certificate. It is safe to add an exception to your browser for https://localhost.

Was this helpful?
What can we do to improve the information ?