Technical FAQs

Ask a Question

Which PDUs are used in the SmartBunker SX and CX?

A customer is asking which PDU is included in the SmartBunker SX and CX. 

Product Line:
SmartBunker SX and CX

All versions and serial ranges.

Customers want to know which PDU comes with the SmartBunker SX or CX. 

PFMSB30024NA ships with AP7902. 
PFMSB30042NA ships with AP8958NA3. 
PFMSB40024NA ships with AP7902 and AP9567. 
PFSMB40038NA ships with AP8958NA3. 
Was this helpful?
What can we do to improve the information ?