Technical FAQs

Ask a Question

Can the Performance Cable Managers and Value Line Cable Managers be installed side by side, or parts be mixed and matched?

Issue:
Customers may want to mix and match parts from these two product families.

Product Line:
NetShelter 2 and 4 Post Open Frame Racks

Environment:
Performance Cable Managers and Value Line Cable Managers

Cause:
Customers with existing cable managers from one product line may want to add managers from the other. Or, customers in the design stage may want to mix and match parts from these two product families.

Resolution:

The Value Line (AR87xx) and Performance (AR86xx) Cable Managers are not compatible.
• They can not be installed side by side. They are different depths so they won’t sit flush and the doors will not open properly.
• The AR8678 and AR8679 End of Row Panels are not compatible with the AR87xx Value Line cable managers.

Was this helpful?
What can we do to improve the information ?