Technical FAQs

Ask a Question

What does “Equivalent Pipe Length” mean?

Issue:
What does “Equivalent Pipe Length” mean?

Product line:
All air cooled cooling units.

Environment:
Data Center Cooling.

Cause:

Resolution:
Equivalent pipe length, EPL is a calculated numeric value that converts the friction losses associated with valves, bends, fittings and fluid velocities to a representative length of straight pipe of a stated type (metal, plastic, etc) and diameter.
 
Was this helpful?
What can we do to improve the information ?