Technical FAQs

Ask a Question

Symmetra PX; invalid IP address when he tried to set network settings in power view display

 
Issue:
Symmetra PX; invalid IP address when he tried to set network settings in power view display
 
Product line:
Symmetra PX, NMC
 
Environment:
All models, all serial numbers
 
Cause:
When configuring the network card setting via the PV display, display shows “invalid IP address” message.
 
Resolution:
Re-boot the NMC card then re-enter the IP configuration settings
 
Was this helpful?
What can we do to improve the information ?